Downloads & Software-Updates
Order No. 0529 00, 2075 00
ZIP, 512.459 Kb
Version: 4.12.0
Date: 30.08.2023
Download
Expert Version 4.12.0
System requirements
- Operating system: Windows 10
- Free hard drive space: at least 1 GB
- RAM: at least 2 GB
- Software platform: at least Microsoft .NET 4.5
Supported devices
The Expert Software 4.12.0 is to be used in conjunction with the following end devices:
- Gira HomeServer 4
- Gira FacilityServer 4
Newness and improvement
Expert/Firmware
- Expert with a new look
- The open visualization is now based on HTML5.
- The logic nodes library has been extended with a Modbus logic node.
- Another logic node enables the integration of the Gira G1.
- The Logic Online Test has been expanded to record the startup sequence.
- Central addresses can now be linked via drag and drop.
- The switching between internal objects and KNX objects in communication objects has been improved.
- Validation of outgoing TLS/HTTPS connections is now possible by adding trusted root certificates in HS/FS.
- In the graphical logic editor, the worksheet can be deactivated.
- Deactivated worksheets can be removed from the transfer to the HS in the graphical logic editor.
- New combined DPTs (RGBW and TBW) for Gira actuators have been added.
- The new Gira switch/blind actuator displays upper and lower end positions.
- Linux components and security patches have been updated to Debian 11.
- Support for TLS v1.3 (HTTPS server) has been added.
- When duplicating an internal communication object, the URL endpoint ID is no longer included.
- The menu item "Window Arrangement" has been moved from "Extras" to "Windows".
- The message "Check the changelog" now also appears when creating new projects.
- The sample project has been revised.
QuadClient
- The floor plan visualization template can now be used as part of the background visualization.
- The timers (QC and Expert) have an additional option to send the current switching state on the bus when the timer is activated.
- The variety of icons in functions and function names has been increased.
- Icons in front of functions in the room can now be activated or deactivated.
- Camera Plugin 2.0 supports full-screen display.
- Audio files can now be played on Windows 10 operating systems and third-party devices.
- The preview images in the plugin selection have been updated.
- When creating a new project, a QC admin with "System Administrator Rights" is automatically added.
- When creating a new project, a menu item for the call list of the building structure is automatically added.
- Plugins can be directly accessed from the main menu with reference to the sub-tab.
- The display of counters, LED indicators, etc. is now also possible in the folder tile in the main menu.
- In "QuadClient Starter," the path of the profiles can be freely determined.
Information
- The ONVIF logic node has been removed from the standard delivery scope as the underlying libraries have been deprecated.
- For the HomeServer update to version 4.12, clients must be updated to at least version 4.12.
- The system has been tested and awarded the VDE security certificate.
Bug fixing
Expert
- The RS flip-flop logic node does not operate as described in the documentation.
- Graphical errors in function templates have been resolved.
- During project validation in HS Expert, the error message "Transmission not possible due to system error.
- The index of the list exceeds the maximum (-1)" appears.
- The sun position logic node (9043) does not correctly evaluate negative values.
- After updating from version 4.9 to 4.11, errors occurred in archive display.
- The NTP server was incomplete. There was an error during project validation.
- There was an error in the help description for presence simulation.
- Importing function templates led to an error message.
- In the help documentation for HS, there was a faulty link in Chapter 1.3.
- The "Max." logic node does not override the current value when the case "/ 0" is output.
- In HS Expert, the text edit logic node does not correctly interpret decimal ASCII values on input 2.
- After a while, the HS always sends the same image by email.
- Symbols in the free visualization change when inserted into another design.
- When DHCP is enabled, the DNS server is not automatically selected.
- After project validation, the error message "kfapperror: Project could not be saved" appears.
- When creating diagrams and inserting archive data, the error message "Could not find archive column" appeared.
- When importing communication objects, the error message "Could not translate internal CO into external" appeared.
- The Maximum Value Comparator logic node had faulty input values (all inputs were 0).
- In recipient groups for email addresses, "oe" was used instead of "ö."
QC
- 1-118 push-button plus – Not all possible symbols are offered.
- Incorrect representation of the KNX smoke detector function template 5-13.
- The status display function template ID 5-55 Version 2.2 from the Gira App Shop displays the wrong version in Experte.
- Function template Switching with Locking Function ID 1-104
- The lock state (ON/OFF) is not displayed in the switching overview.
- The diagram plugin lacks a default color, causing lines to be mostly drawn in black or white by apps.
- Music control function template 5-91 - Translation error in English.
- The Basic Plan Editor plugin can be started multiple times.
- In the push-button plus function template 1-118, with active PIN protection, no padlock symbol is displayed.
- List Plus function template ID 5-87 - Faulty display in the iOS app.
- The Meldeanlage plugin from the Gira App Shop does not support a white design.
- Calling a specific tab through the menu item does not work.
- Duplicating a function template changes the group address of the original when adjustments are made to the duplicate.
- The floor plan editor does not display the complete building structure.
- When using a background image in the room in QuadConfig, it is only partially displayed in the light design.
- In the camera plugin, a timeout occurs after the power-saving mode.
- The QC (QuadConfig) cannot be closed. The status symbol "Fireplace On/Off" is identical.
- In the music control function template 5-91 and the Universal Player plugin 1-25, the display of the play/pause buttons is opposite.
- In Camera Plugin 2.0, a still image is displayed after a certain period of time.
- The font is incorrect when the trades view is first opened.
- The representation of the symbol pool is faulty.
- In the heating setpoint adjustment function template, the temperature drops to the minimum when the slider is tapped.
- The Fan Coil function template 5-0 crashes when "Circulation Off" is pressed.
- The socket symbol in the function template "1-101" is faulty.
- In the function template "1-125 Value Input Plus," negative numbers can be entered.
- The slider in the heating template "1-122" does not work correctly.
iOS App
- The app displays the remote access activation mode.
- Camera Plugin 2.0 - Camera image is delayed and doesn't refresh.
- Mobotix camera is not appearing in the plugin.
- Merging profiles no longer functions.
- No functionality through LAN connection.
- No camera image in the plugin with Basic Authentication.
- Parser Error after minor project changes in QC.
- Timing issue when calling up the profile, interruption during retrieval on WLAN or via S1.
- No direct display when a camera is added in the plugin.
- Loadgroups Error has been resolved.
- Push notifications stop working after X days.
- Functional templates from Gira App Shop - missing symbols.
- When calling up a plugin in a submenu, the back button becomes grayed out.
- No connection possible through port forwarding, faulty behavior at the Maldives location.
Android App/Gira G1
- In the menu item "Status display as counter," when it's configured as green, it is displayed as gray.
- When using the "Value Display / Weather Station" plugin and selecting the "TEXT" format, Android devices display "TEXT0" instead of the sent text.
- Android users see areas for which they don't have permission.
- The speed of camera images has been improved.
- The reconnect popup remains in the foreground.
- Samsung devices show a red background.
- The client displays an incorrect time format.
- Status symbols do not switch, for example, the door always stays on "unlocked" in the app.
- In the 1-128 Tunable White Template, saving the new color value does not work in memory.
- An error message "LPNS Error Push Message" occurs when there is no internet available.
- In Camera Plugin 2.0, the camera image is repeatedly displayed as a still image.
- The buttons within the Camera Plugin 2.0 do not work when the set value command is executed.
- When calling up trades, there is sluggish behavior.
- The representation of the symbol pool is faulty.
- In the functional template "Heating Setpoint Adjustment," the temperature resets to the minimum when tapping the slider.
- The functional template "Fan Coil 5-0" crashes when "Circulation Off" is pressed.
- The socket symbol in the functional template "1-101" is faulty.
- In the functional template "1-125 Value Input Plus," negative numbers can be entered.
- The slider in the functional template "Heating 1-122" does not function correctly.
Other
- No devices are found in the Alexa integration.
- The logic node "Door analysis 5fach" responds to all fingers.
Known errors
- Logic node "Dornbracht SmartWater" help text cannot be opened in the graphical logic editor.
- Logic node "Status Forwarding Evaluation" is not taken into account.
- Quad Config: When creating a function template directly in the trade, it is not possible to activate the timer directly via QC on the PC or via CO.
- Quad Config: Operation by keyboard instead of mouse leads to QC Config crash.
- Quad Client QC: Missing symbols or controls, red squares e.g. with project changes or extensions in App Shop templates.
- Quad Client QC: Multilingualism is activated and menu or function labels are changed without effect.
- Quad Client: Function template 1-125 Value Input Plus & communication object with 32-bit data type experiences an error.
- Android App: Missing symbols or controls, red squares with project changes or extensions in App Shop templates.
- Android App: Camera 2.0 Plugin - No image display in single view - Additional sub-element must be used for an image to be displayed.
- iOS App: Incorrect representation of time information.