Downloads & Software-Updates


Category

Gira Expert

back

Order No. 0529 00, 2075 00

ZIP, 458.819 Kb

Version: 4.11.0

Date: 07.12.2020

Download

Archive

Language variants

Experte Version 4.11.0

System requirements

  • Operating system: Windows 7, Windows 8, Windows 10
  • Free hard drive space: at least 1 GB
  • RAM: at least 2 GB
  • Software platform: at least Microsoft .NET 4.5

Supported devices

The Expert Software 4.11.0 is to be used in conjunction with the following end devices:

  • Gira HomeServer 4
  • Gira FacilityServer 4

Update information

It is only possible to update to firmware version 4.11.0 from the following version:

  • 4.10.1.200330
  • 4.10.0.200117
  • 4.9.0.190612

New products and improvements

Expert/firmware

  • Logic online test in the graphical logic editor
  • Simplification of the configuration
  • Connection to Gira Alarm Connect
  • DHCP
    DHCP can be set under the project settings / network.
  • Revised scene node
  • Home page
    An overview page with all the available URL call-ups is now displayed when the IP address of the HomeServer is entered.

QuadClient

  • Day/night switch-over
    The QuadClient can be switched between day (bright design) and night (dark design).
  • New symbols
  • Floor plan navigation
  • Floor plan editor
  • Alarm plug-in

Bug fixes

  • Project transfer dialogue not always in the background
  • Scenes logic node - faulty translation fixed
  • Expert - no error message after project import to missing HSLX files
  • Expert - error message issued if “forbidden” port has been set
  • Expert - images/symbols from global library are not displayed correctly or are mixed up in Design 1920x1080V
  • The error has been fixed in version 4.11.0. However, if a global library of an older expert version is imported, the error may reoccur because the global libraries of the older version are also affected by the error.
  • Expert - visualisation of dynamic texts - if “Call up last settings” is not set, the dialogue is shown again in the visualisation when setting up dynamic texts.
  • Expert - visualisation - “smaller than” character “<” is no longer displayed as “[”.
  • HS Client - GIFs were not able to be selected in the HS Client under certain circumstances (error fixed)
  • Logic node - “selector switch” input - error at input 2 fixed
  • QuadClient - weather forecast plug-in - refresh within specified time again
  • QuadClient - template definition in Design 5, centred display adapted for iOS
  • QuadClient - the return times for MyTouch are now permanently applied
  • QuadClient - function template Push-button Plus (ID 1-118) with PIN protection adapted
  • QuadClient - timer in QC Dimming Plus adapted

Known errors

  • DCS communicator - Show and Hide commands under Windows 10
  • HomeServer / S1 - camera access from external point does not work correctly
  • HS QC call-up from specific tab via menu item does not work
  • Logic node: “Evaluate forwarding status”
  • S1 Windows Client - HS free visualisation call-up in browser - the certificate is not recognised
  • QC configuration - umlauts in the user name

Gira verwendet Cookies für Websites in der Domain gira.de. Einige von ihnen sind essenziell, während andere uns helfen, diese Website und Ihre Erfahrung zu verbessern. Erfahren Sie mehr zu den von uns oder Dritten eingesetzten Cookies und Ihren Möglichkeiten diese auszustellen in unserer Datenschutzerklärung.

Wenn Sie Cookies zur statistischen Auswertung ablehnen, werden keine Tracking Cookies gesendet. Ihr Besuch auf dieser Website wird dann nicht erfasst.