Downloads & Software-Updates


Category

Gira surface-mounted video home station 7

back

Order No. 1209 ..

ZIP, 173.728 Kb

Version: 1.0.42

Date: 02.05.2019

Download

Language variants

Important Information

Prerequisites for the commissioning of the surface-mounted video home station 7 using the Gira Project Assistant:

  • GPA as of version 3.4
  • DCS-IP-data-interface as of version 1.1
  • Surface-mounted video home station 7 as of version 1.0.42

Errors fixed

  • The settings for the parameter "Main screen" are now copied correctly in the surface-mounted video home station 7 when parametrising via Gira Project Assistant.
  • The settings for the parameter "Activate resistance" are now copied correctly in the surface-mounted video home station 7 when parametrising via Gira Project Assistant.
  • During parametrising with Gira Project Assistant, the Gira logo as well as the localised term "Commissioning ..." are displayed with the surface-mounted video home station 7.
    The slider for the "Voice volume" is now displayed correctly after a reboot.
  • The slider "Pause between images captured" in the Image memory menu remains operable even with the parameter "Number of images upon door opening" = 1.
  • The displayed image quality of the saved images in the Image memory menu now equals the quality of the live image as well as the saved JPEG photos.

Information on firmware update

  • For the firmware update you need a microSD card formatted to FAT32 with at least 500 MB memory.
  • Create a folder with the name "update" on the microSD card.
  • Download the ZIP file with the file for the firmware update from the Gira download area.
  • Copy the file (.swu) for the firmware update from the ZIP file into the folder "update" on the microSD card.
  • At the home station, access the "Settings" menu, select "Update" and follow the instructions of the Assistant.
  • Please note: The update function may need to be enabled first by the installer.